Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static LaminateImportedLayupBuilder.ImportMethodEnum |
LaminateImportedLayupBuilder.ImportMethodEnum.EXTERNAL_API
External API.
|
static LaminateImportedLayupBuilder.ImportMethodEnum |
LaminateImportedLayupBuilder.ImportMethodEnum.EXTERNAL_FILE
External file.
|
Modifier and Type | Method and Description |
---|---|
LaminateImportedLayupBuilder.ImportMethodEnum |
LaminateImportedLayupBuilder.importMethod()
Returns the import method
License requirements: None. |
static LaminateImportedLayupBuilder.ImportMethodEnum |
LaminateImportedLayupBuilder.ImportMethodEnum.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LaminateImportedLayupBuilder.ImportMethodEnum |
LaminateImportedLayupBuilder.ImportMethodEnum.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LaminateImportedLayupBuilder.ImportMethodEnum[] |
LaminateImportedLayupBuilder.ImportMethodEnum.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LaminateImportedLayupBuilder.setImportMethod(LaminateImportedLayupBuilder.ImportMethodEnum importMethod)
License requirements: nx_lam_comp_adv ("Laminate Composites Advanced") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.