Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Method and Description |
---|---|
LaminateGraphicalReport |
LaminateGraphicalReportCollection.findObject(String name)
Finds a laminate graphical post report with the specified name
License requirements: nx_lam_composites ("Laminate Composites") . |
Modifier and Type | Method and Description |
---|---|
void |
LaminateGraphicalReportCollection.cloneReport(LaminateGraphicalReport graphicalReport)
Clone a laminate graphical post report
License requirements: nx_lam_composites ("Laminate Composites") . |
LaminateGraphicalReportBuilder |
LaminatePostReportCollection.createLaminateGraphicalReportBuilder(LaminateGraphicalReport graphicalReport)
Creates the builder for the
LaminateGraphicalReport class
License requirements: nx_lam_composites ("Laminate Composites") Created in NX8.0.0 |
SolutionResult |
ResultManager.createLaminateGraphicalReportResult(LaminateGraphicalReport lamGraphReport)
Creates a solution result object given a
LaminateGraphicalReport
It is user's responsibility to destroy the result object once done
using ResultManager.deleteResult(nxopen.cae.Result) , in order to free up system resources. |
void |
LaminateGraphicalReportCollection.deleteReport(LaminateGraphicalReport graphicalReport)
Delete a laminate graphical post report
License requirements: nx_lam_composites ("Laminate Composites") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.