Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Interface and Description |
---|---|
interface |
LaminateRandomEvent
The Laminate Dynamic Event.
|
interface |
LaminateSineEvent
The Laminate Sine Event.
|
Modifier and Type | Method and Description |
---|---|
LaminateDynamicEvent |
LaminateDynamicEventCollection.findObject(String name)
Finds a laminate dynamic event with the specified name
License requirements: nx_lam_comp_adv ("Laminate Composites Advanced") . |
Modifier and Type | Method and Description |
---|---|
void |
LaminateDynamicEventCollection.cloneDynamicEvent(LaminateDynamicEvent dynamicEvent)
Clones the laminate dynamic event
License requirements: nx_lam_comp_adv ("Laminate Composites Advanced") . |
SolutionResult |
ResultManager.createLaminateDynamicEventResult(LaminateDynamicEvent dynEvent)
Creates a solution result object given a
LaminateDynamicEvent
It is user's responsibility to destroy the result object once done
using ResultManager.deleteResult(nxopen.cae.Result) , in order to free up system resources. |
void |
LaminateDynamicEventCollection.delete(LaminateDynamicEvent dynamicEvent)
Deletes the laminate dynamic event
License requirements: nx_lam_comp_adv ("Laminate Composites Advanced") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.