Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static ImprintBuilder.ProjectionDirectionType |
ImprintBuilder.ProjectionDirectionType.ALONG_VECTOR |
static ImprintBuilder.ProjectionDirectionType |
ImprintBuilder.ProjectionDirectionType.NATURAL_EXTENSION |
Modifier and Type | Method and Description |
---|---|
ImprintBuilder.ProjectionDirectionType |
ImprintBuilder.projectionDirectionMethod()
Returns the projection direction method
License requirements: None. |
static ImprintBuilder.ProjectionDirectionType |
ImprintBuilder.ProjectionDirectionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ImprintBuilder.ProjectionDirectionType |
ImprintBuilder.ProjectionDirectionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ImprintBuilder.ProjectionDirectionType[] |
ImprintBuilder.ProjectionDirectionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ImprintBuilder.setProjectionDirectionMethod(ImprintBuilder.ProjectionDirectionType projDirectionType)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.