Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static FluidDomainBuilder.IntExtType |
FluidDomainBuilder.IntExtType.CAVITY_POINTS
The interior specified by cavity points.
|
static FluidDomainBuilder.IntExtType |
FluidDomainBuilder.IntExtType.FACE_AND_NORMAL_VECTOR
The interior specified by providing a face and a normal.
|
static FluidDomainBuilder.IntExtType |
FluidDomainBuilder.IntExtType.FROM_EXTERIOR
Wrap from the exterior.
|
static FluidDomainBuilder.IntExtType |
FluidDomainBuilder.IntExtType.POINT
The interior specified by providing a point.
|
Modifier and Type | Method and Description |
---|---|
FluidDomainBuilder.IntExtType |
FluidDomainBuilder.interiorExteriorType()
Returns the interior selection type represented by
FluidDomainBuilder.IntExtType
License requirements: None. |
static FluidDomainBuilder.IntExtType |
FluidDomainBuilder.IntExtType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FluidDomainBuilder.IntExtType |
FluidDomainBuilder.IntExtType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FluidDomainBuilder.IntExtType[] |
FluidDomainBuilder.IntExtType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FluidDomainBuilder.setInteriorExteriorType(FluidDomainBuilder.IntExtType type)
License requirements: nx_adv_fluid_mod ("NX Advanced Fluid Modeling - Basic") OR sc_acou_meshing (" SC Acoustic Meshing") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.