Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static FemSignalProcessingSignalAttributes.SpectrumScalings |
FemSignalProcessingSignalAttributes.SpectrumScalings.PEAK
Peak
|
static FemSignalProcessingSignalAttributes.SpectrumScalings |
FemSignalProcessingSignalAttributes.SpectrumScalings.RMS
RMS
|
static FemSignalProcessingSignalAttributes.SpectrumScalings |
FemSignalProcessingSignalAttributes.SpectrumScalings.UNKNOWN
Unkonwn
|
Modifier and Type | Method and Description |
---|---|
FemSignalProcessingSignalAttributes.SpectrumScalings |
FemSignalProcessingSignalAttributes.spectrumScaling()
Returns the spectrum scaling in which the data is encoded.
|
static FemSignalProcessingSignalAttributes.SpectrumScalings |
FemSignalProcessingSignalAttributes.SpectrumScalings.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FemSignalProcessingSignalAttributes.SpectrumScalings |
FemSignalProcessingSignalAttributes.SpectrumScalings.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FemSignalProcessingSignalAttributes.SpectrumScalings[] |
FemSignalProcessingSignalAttributes.SpectrumScalings.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
FemSignalProcessingSignalAttributes |
FemSignalProcessingApplication.createSignalAttributes(FemSignalProcessingSignalAttributes.SpectrumScalings defaultVisualizationSpectrumScaling,
FemSignalProcessingSignalAttributes.CorrectionModes defaultVisualizationCorrectionMode,
double amplitudeCorrectionFactor,
double energyCorrectionFactor,
FemSignalProcessingSignalAttributes.AcousticalWeightings acousticalWeighting)
Creates a new set of signal attributes that can be attached to a field.
|
void |
FemSignalProcessingSignalAttributes.setSpectrumScaling(FemSignalProcessingSignalAttributes.SpectrumScalings spectrumScaling)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.