Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static FemSignalProcessingSignalAttributes.CorrectionModes |
FemSignalProcessingSignalAttributes.CorrectionModes.AMPLITUDE
Amplitude
|
static FemSignalProcessingSignalAttributes.CorrectionModes |
FemSignalProcessingSignalAttributes.CorrectionModes.ENERGY
Energy
|
static FemSignalProcessingSignalAttributes.CorrectionModes |
FemSignalProcessingSignalAttributes.CorrectionModes.UNKNOWN
Unkonwn
|
Modifier and Type | Method and Description |
---|---|
FemSignalProcessingSignalAttributes.CorrectionModes |
FemSignalProcessingSignalAttributes.correctionMode()
Returns the correction mode in which the data is encoded
License requirements: None. |
static FemSignalProcessingSignalAttributes.CorrectionModes |
FemSignalProcessingSignalAttributes.CorrectionModes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FemSignalProcessingSignalAttributes.CorrectionModes |
FemSignalProcessingSignalAttributes.CorrectionModes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FemSignalProcessingSignalAttributes.CorrectionModes[] |
FemSignalProcessingSignalAttributes.CorrectionModes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
FemSignalProcessingSignalAttributes |
FemSignalProcessingApplication.createSignalAttributes(FemSignalProcessingSignalAttributes.SpectrumScalings defaultVisualizationSpectrumScaling,
FemSignalProcessingSignalAttributes.CorrectionModes defaultVisualizationCorrectionMode,
double amplitudeCorrectionFactor,
double energyCorrectionFactor,
FemSignalProcessingSignalAttributes.AcousticalWeightings acousticalWeighting)
Creates a new set of signal attributes that can be attached to a field.
|
void |
FemSignalProcessingSignalAttributes.setCorrectionMode(FemSignalProcessingSignalAttributes.CorrectionModes correctionMode)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.