Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Method and Description |
---|---|
FeatureNodeMethod |
SmartSelectionManager.createFeatureNodeMethod(FEElement[] seedTags,
int[] seedElemFaceIds,
double dFeatureAngle)
Deprecated.
Deprecated in NX10.0.0. Use overloaded
SmartSelectionManager.createFeatureNodeMethod(nxopen.cae.FEElement, int, double) which takes as input an array of FEElement objects and the argument doEntityVisibilityCheck.
|
FeatureNodeMethod |
SmartSelectionManager.createFeatureNodeMethod(FEElement seedElemTag,
int seedElemFaceId,
double dFeatureAngle)
Deprecated.
Deprecated in NX10.0.0. Use overloaded
SmartSelectionManager.createFeatureNodeMethod(nxopen.cae.FEElement, int, double) which takes as input an array of FEElement objects and the argument doEntityVisibilityCheck.
|
FeatureNodeMethod |
SmartSelectionManager.createFeatureNodeMethod(FEElemFace[] seedTags,
boolean doEntityVisibilityCheck,
boolean computeFreeFacesOnVisibleModel,
boolean stopAtNonManifoldJunctions,
double dFeatureAngle)
Creates a feature node method
License requirements: nx_masterfem ("Finite Element Modeling") . |
FeatureNodeMethod |
SmartSelectionManager.createFeatureNodeMethod(FEElemFace[] seedTags,
boolean doEntityVisibilityCheck,
boolean computeFreeFacesOnVisibleModel,
double dFeatureAngle)
Deprecated.
Deprecated in NX12.0.0. Use overloaded
SmartSelectionManager.createFeatureNodeMethod(nxopen.cae.FEElement, int, double) which takes as input argument stopAtNonManifoldJunctions.
|
FeatureNodeMethod |
SmartSelectionManager.createFeatureNodeMethod(FEElemFace[] seedTags,
double dFeatureAngle)
Deprecated.
Deprecated in NX11.0.0. Use overloaded
SmartSelectionManager.createFeatureNodeMethod(nxopen.cae.FEElement, int, double) which takes as input an array of FEElemFace objects and the argument doEntityVisibilityCheck.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.