Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Method and Description |
---|---|
FeatureElemEdgeMethod |
SmartSelectionManager.createFeatureElemEdgeMethod(FEElemEdge[] seedTags,
boolean doEntityVisibilityCheck,
boolean computeFreeEdgesOnVisibleModel,
boolean stopAtNonManifoldJunctions,
Type edgeType,
double dFeatureAngle)
Creates a feature elem edge method
License requirements: nx_masterfem ("Finite Element Modeling") . |
FeatureElemEdgeMethod |
SmartSelectionManager.createFeatureElemEdgeMethod(FEElemEdge[] seedTags,
boolean doEntityVisibilityCheck,
boolean computeFreeEdgesOnVisibleModel,
double dFeatureAngle)
Deprecated.
Deprecated in NX12.0.0. Use overloaded
SmartSelectionManager.createFeatureElemEdgeMethod(nxopen.cae.FEElement, int, double) which takes as input an array of FEElemEdge or Mesh objects and the argument edgeType.
|
FeatureElemEdgeMethod |
SmartSelectionManager.createFeatureElemEdgeMethod(FEElemEdge[] seedTags,
double dFeatureAngle)
Deprecated.
Deprecated in NX11.0.0. Use overloaded
SmartSelectionManager.createFeatureElemEdgeMethod(nxopen.cae.FEElement, int, double) which takes as input an array of FEElemEdge objects and the argument doEntityVisibilityCheck.
|
FeatureElemEdgeMethod |
SmartSelectionManager.createFeatureElemEdgeMethod(FEElement[] seedTags,
int[] seedElemEdgeIds,
double dFeatureAngle)
Deprecated.
Deprecated in NX10.0.0. Use overloaded
SmartSelectionManager.createFeatureElemEdgeMethod(nxopen.cae.FEElement, int, double) which takes as input an array of FEElement objects and the argument doEntityVisibilityCheck.
|
FeatureElemEdgeMethod |
SmartSelectionManager.createFeatureElemEdgeMethod(FEElement seedElemTag,
int seedElemEdgeId,
double dFeatureAngle)
Deprecated.
Deprecated in NX10.0.0. Use overloaded
SmartSelectionManager.createFeatureElemEdgeMethod(nxopen.cae.FEElement, int, double) which takes as input an array of FEElement objects and the argument doEntityVisibilityCheck.
|
FeatureElemEdgeMethod |
SmartSelectionManager.createFeatureElemEdgeMethod(Mesh[] seedTags,
boolean doEntityVisibilityCheck,
boolean computeFreeEdgesOnVisibleModel,
boolean stopAtNonManifoldJunctions,
Type edgeType,
double dFeatureAngle)
Creates a feature elem edge method
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.