Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Method and Description |
---|---|
FEModelOccurrence |
SimSimulation.femodel()
Returns the FEModelOccurrence
FEModelOccurrence associated with the simulation object
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") Created in NX5.0.0 |
FEModelOccurrence[] |
IHierarchicalFEModel.getChildren()
Returns the child components of this component
License requirements: None. |
FEModelOccurrence |
AssyFEModel.getMappedFemOccForAssemblyComponent(Component cadPartOcc)
Returns the
FEModelOccurrence in this assembly fem that corresponds to an Component . |
FEModelOccurrence |
AssyFEModel.mapFemToAssemblyComponent(BaseFemPart femPart,
Component cadPartOcc,
boolean workLayer)
Map a fem part to an assembly component in an assembly fem.
|
FEModelOccurrence[] |
AssyFEModel.mapFemToMultiAssemblyComponents(BaseFemPart femPart,
Component[] pCadPartOccs,
boolean workLayer)
Map a fem part to multiple assembly components in an assembly fem.
|
Modifier and Type | Method and Description |
---|---|
void |
SimLoadRecipe.autofill(FEModelOccurrence feModelOcc)
Deprecated.
Deprecated in NX12.0.0. Use
SimLoadRecipe.autofill() instead.
|
Component |
AssyFEModel.getAssemblyComponentForMappedFemOcc(FEModelOccurrence femOcc)
Returns the
Component in the Cad assembly fem that corresponds to an FEModelOccurrence . |
SimPart.ImportErrorCodes |
SimPart.importSim(String fileName,
String prependString,
SimPart.ImportOptions selOptions,
FEModelOccurrence[] selectedFemoccs)
Imports all entities of selected type from the source sim into the current (target) sim.
|
void |
SimLoadRecipe.setAutofillAssemblyComponent(FEModelOccurrence feModelOcc)
Set the assembly component on which the autofill method operates on.
|
void |
ImportSimulationBuilder.setTargetFemoccs(FEModelOccurrence[] selectedFemoccs)
Set FeModel Occurrences to import onto
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.