Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static FEModelOccAttribute.RepType |
FEModelOccAttribute.RepType.BASE_FEM
No alternate rep.
|
static FEModelOccAttribute.RepType |
FEModelOccAttribute.RepType.SUPER_ELEMENT
Alternate rep is a superelement
|
Modifier and Type | Method and Description |
---|---|
FEModelOccAttribute.RepType |
FEModelOccAttribute.getRepType()
Get the representation type on the attribute (base_fem or super element)
License requirements: nx_masterfem ("Finite Element Modeling") . |
static FEModelOccAttribute.RepType |
FEModelOccAttribute.RepType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FEModelOccAttribute.RepType |
FEModelOccAttribute.RepType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FEModelOccAttribute.RepType[] |
FEModelOccAttribute.RepType.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.