Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static ElementTranslateBuilder.MethodType |
ElementTranslateBuilder.MethodType.COMPONENT
translate by components
|
static ElementTranslateBuilder.MethodType |
ElementTranslateBuilder.MethodType.DIRECTION
translate along a vector
|
static ElementTranslateBuilder.MethodType |
ElementTranslateBuilder.MethodType.ELEM_NORMAL
translate along element normal
|
static ElementTranslateBuilder.MethodType |
ElementTranslateBuilder.MethodType.POINT_TO_POINT
translate by point to point
|
Modifier and Type | Method and Description |
---|---|
ElementTranslateBuilder.MethodType |
ElementTranslateBuilder.method()
Returns the method to be used for translating the selected elements
License requirements: None. |
static ElementTranslateBuilder.MethodType |
ElementTranslateBuilder.MethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ElementTranslateBuilder.MethodType |
ElementTranslateBuilder.MethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ElementTranslateBuilder.MethodType[] |
ElementTranslateBuilder.MethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ElementTranslateBuilder.setMethod(ElementTranslateBuilder.MethodType method)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.