Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static ElementTranslateBuilder.CopyType |
ElementTranslateBuilder.CopyType.COPY_TRANSLATE
first copy elements then translate the copies
|
static ElementTranslateBuilder.CopyType |
ElementTranslateBuilder.CopyType.ELEMENT_COAT
make 1D element using the existing nodes
|
static ElementTranslateBuilder.CopyType |
ElementTranslateBuilder.CopyType.TRANSLATE_ONLY
translate without copying elements
|
Modifier and Type | Method and Description |
---|---|
ElementTranslateBuilder.CopyType |
ElementTranslateBuilder.copyOption()
Returns the copy option .
|
static ElementTranslateBuilder.CopyType |
ElementTranslateBuilder.CopyType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ElementTranslateBuilder.CopyType |
ElementTranslateBuilder.CopyType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ElementTranslateBuilder.CopyType[] |
ElementTranslateBuilder.CopyType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ElementTranslateBuilder.setCopyOption(ElementTranslateBuilder.CopyType inCopyoption)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.