Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static ElementRotateBuilder.NewMeshType |
ElementRotateBuilder.NewMeshType.CREATE
create a new mesh
|
static ElementRotateBuilder.NewMeshType |
ElementRotateBuilder.NewMeshType.EXISTING
add new elements to an existing mesh
|
Modifier and Type | Method and Description |
---|---|
ElementRotateBuilder.NewMeshType |
ElementRotateBuilder.newMeshOption()
Returns the option to create a new mesh or add the new elements to an existing mesh
License requirements: None. |
static ElementRotateBuilder.NewMeshType |
ElementRotateBuilder.NewMeshType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ElementRotateBuilder.NewMeshType |
ElementRotateBuilder.NewMeshType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ElementRotateBuilder.NewMeshType[] |
ElementRotateBuilder.NewMeshType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ElementRotateBuilder.setNewMeshOption(ElementRotateBuilder.NewMeshType newMeshOption)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.