Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static ElementRotateBuilder.ElemDimensionType |
ElementRotateBuilder.ElemDimensionType.ANY
any element can be selected
|
static ElementRotateBuilder.ElemDimensionType |
ElementRotateBuilder.ElemDimensionType.BEAM
only beam elements can be selected
|
static ElementRotateBuilder.ElemDimensionType |
ElementRotateBuilder.ElemDimensionType.SHELL
only shell elements can be selected
|
static ElementRotateBuilder.ElemDimensionType |
ElementRotateBuilder.ElemDimensionType.SOLID
only solid elements can be selected
|
Modifier and Type | Method and Description |
---|---|
ElementRotateBuilder.ElemDimensionType |
ElementRotateBuilder.elementDimension()
Returns the dimension of the elements to be rotated
License requirements: None. |
static ElementRotateBuilder.ElemDimensionType |
ElementRotateBuilder.ElemDimensionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ElementRotateBuilder.ElemDimensionType |
ElementRotateBuilder.ElemDimensionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ElementRotateBuilder.ElemDimensionType[] |
ElementRotateBuilder.ElemDimensionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ElementRotateBuilder.setElementDimension(ElementRotateBuilder.ElemDimensionType elementDimension)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.