Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static ElementRotateBuilder.DistanceType |
ElementRotateBuilder.DistanceType.PER_COPY
distance specified is for each copy
|
static ElementRotateBuilder.DistanceType |
ElementRotateBuilder.DistanceType.TOTAL
distance specified is total translation distance
|
Modifier and Type | Method and Description |
---|---|
ElementRotateBuilder.DistanceType |
ElementRotateBuilder.distanceCopyOption()
Returns the distance option
License requirements: None. |
static ElementRotateBuilder.DistanceType |
ElementRotateBuilder.DistanceType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ElementRotateBuilder.DistanceType |
ElementRotateBuilder.DistanceType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ElementRotateBuilder.DistanceType[] |
ElementRotateBuilder.DistanceType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ElementRotateBuilder.setDistanceCopyOption(ElementRotateBuilder.DistanceType distanceOption)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.