Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Method and Description |
---|---|
ElemEdgePathMethod |
SmartSelectionManager.createElemEdgePathMethod(FEElemEdge seedElemEdgeTag,
FENode seedStartNodeTag)
Deprecated.
Deprecated in NX10.0.0. Use overloaded
SmartSelectionManager.createElemEdgePathMethod(nxopen.cae.FEElemEdge, nxopen.cae.FENode) which takes as input an array of FEElemEdge objects and the argument doEntityVisibilityCheck.
|
ElemEdgePathMethod |
SmartSelectionManager.createElemEdgePathMethod(FEElemEdge seedElemEdgeTag,
FENode seedStartNodeTag,
boolean preferFreeEdges,
boolean preferGeometryAssociatedEdges,
boolean preferFeatureElementEdge,
double featureAngleTolerance,
boolean allowGapJumping,
double gapJumpingTolerance)
Creates an elem edge path method
License requirements: nx_masterfem ("Finite Element Modeling") . |
Modifier and Type | Method and Description |
---|---|
void |
MeshFromBoundaryBuilder.setSourceElementEdgePathMethod(ElemEdgePathMethod sourceElementEdgePathMethod)
Set the source element path of the selection
License requirements: nx_masterfem ("Finite Element Modeling") . |
void |
MeshFromBoundaryBuilder.setTargetElementEdgePathMethod(ElemEdgePathMethod targetElementEdgePathMethod)
Set the target elemnt path of the selection
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.