Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static EdgeSticherBuilder.Types |
EdgeSticherBuilder.Types.AUTOMATIC_FREE_EDGE_TO_ALL_EDGES |
static EdgeSticherBuilder.Types |
EdgeSticherBuilder.Types.MANUAL_EDGE_TO_EDGE |
static EdgeSticherBuilder.Types |
EdgeSticherBuilder.Types.MANUAL_EDGE_TO_FACE |
Modifier and Type | Method and Description |
---|---|
EdgeSticherBuilder.Types |
EdgeSticherBuilder.type()
Returns the type : (Obsolete from NX07.5 onwards)
License requirements: None. |
static EdgeSticherBuilder.Types |
EdgeSticherBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EdgeSticherBuilder.Types |
EdgeSticherBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EdgeSticherBuilder.Types[] |
EdgeSticherBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EdgeSticherBuilder.setType(EdgeSticherBuilder.Types type)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.