Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static EdgeFaceImprintBuilder.ProjectionDirectionType |
EdgeFaceImprintBuilder.ProjectionDirectionType.ALONG_NORMAL |
static EdgeFaceImprintBuilder.ProjectionDirectionType |
EdgeFaceImprintBuilder.ProjectionDirectionType.ALONG_VECTOR |
static EdgeFaceImprintBuilder.ProjectionDirectionType |
EdgeFaceImprintBuilder.ProjectionDirectionType.CLOSET_TO_TARGET |
Modifier and Type | Method and Description |
---|---|
EdgeFaceImprintBuilder.ProjectionDirectionType |
EdgeFaceImprintBuilder.projectionDirectionMethod()
Returns the projection direction method
License requirements: None. |
static EdgeFaceImprintBuilder.ProjectionDirectionType |
EdgeFaceImprintBuilder.ProjectionDirectionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EdgeFaceImprintBuilder.ProjectionDirectionType |
EdgeFaceImprintBuilder.ProjectionDirectionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EdgeFaceImprintBuilder.ProjectionDirectionType[] |
EdgeFaceImprintBuilder.ProjectionDirectionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EdgeFaceImprintBuilder.setProjectionDirectionMethod(EdgeFaceImprintBuilder.ProjectionDirectionType projDirectionType)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.