Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static DurabilityStrainGageAnalyzerBuilder.CriticalPlaneOptionEnum |
DurabilityStrainGageAnalyzerBuilder.CriticalPlaneOptionEnum.MAXIMUM_PRINCIPAL
Maximum Principal
|
static DurabilityStrainGageAnalyzerBuilder.CriticalPlaneOptionEnum |
DurabilityStrainGageAnalyzerBuilder.CriticalPlaneOptionEnum.MAXIMUM_SHEAR
Maximum Shear
|
Modifier and Type | Method and Description |
---|---|
DurabilityStrainGageAnalyzerBuilder.CriticalPlaneOptionEnum |
DurabilityStrainGageAnalyzerBuilder.criticalPlaneOption()
Returns the critical plane option.
|
static DurabilityStrainGageAnalyzerBuilder.CriticalPlaneOptionEnum |
DurabilityStrainGageAnalyzerBuilder.CriticalPlaneOptionEnum.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DurabilityStrainGageAnalyzerBuilder.CriticalPlaneOptionEnum |
DurabilityStrainGageAnalyzerBuilder.CriticalPlaneOptionEnum.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DurabilityStrainGageAnalyzerBuilder.CriticalPlaneOptionEnum[] |
DurabilityStrainGageAnalyzerBuilder.CriticalPlaneOptionEnum.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DurabilityStrainGageAnalyzerBuilder.setCriticalPlaneOption(DurabilityStrainGageAnalyzerBuilder.CriticalPlaneOptionEnum criticalPlaneOption)
License requirements: nx_adv_durability ("NX Advanced Durability") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.