Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static DurabilityResultsReportBuilder.UseEventsEnum |
DurabilityResultsReportBuilder.UseEventsEnum.ACTIVE |
static DurabilityResultsReportBuilder.UseEventsEnum |
DurabilityResultsReportBuilder.UseEventsEnum.ALL |
Modifier and Type | Method and Description |
---|---|
DurabilityResultsReportBuilder.UseEventsEnum |
DurabilityResultsReportBuilder.useEvents()
Returns the use events pop-up menu
License requirements: None. |
static DurabilityResultsReportBuilder.UseEventsEnum |
DurabilityResultsReportBuilder.UseEventsEnum.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DurabilityResultsReportBuilder.UseEventsEnum |
DurabilityResultsReportBuilder.UseEventsEnum.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DurabilityResultsReportBuilder.UseEventsEnum[] |
DurabilityResultsReportBuilder.UseEventsEnum.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DurabilityResultsReportBuilder.setUseEvents(DurabilityResultsReportBuilder.UseEventsEnum useEvents)
License requirements: nx_adv_durability ("NX Advanced Durability") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.