Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static DurSpecialistLocalDefinitionBuilder.LocationType |
DurSpecialistLocalDefinitionBuilder.LocationType.SPECIFY
Specify location
|
static DurSpecialistLocalDefinitionBuilder.LocationType |
DurSpecialistLocalDefinitionBuilder.LocationType.USE_REMAINING_STRUCTURE
Use the remaining structure
|
Modifier and Type | Method and Description |
---|---|
DurSpecialistLocalDefinitionBuilder.LocationType |
DurSpecialistLocalDefinitionBuilder.location()
Returns the location
License requirements: None. |
static DurSpecialistLocalDefinitionBuilder.LocationType |
DurSpecialistLocalDefinitionBuilder.LocationType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DurSpecialistLocalDefinitionBuilder.LocationType |
DurSpecialistLocalDefinitionBuilder.LocationType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DurSpecialistLocalDefinitionBuilder.LocationType[] |
DurSpecialistLocalDefinitionBuilder.LocationType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DurSpecialistLocalDefinitionBuilder.setLocation(DurSpecialistLocalDefinitionBuilder.LocationType type)
License requirements: nx_adv_durability ("NX Advanced Durability") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.