Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Method and Description |
---|---|
DependentMeshListItemBuilder |
DependentMeshBuilder.createNewListItem(CAEEdge tMasterEdge,
CAEEdge tTargetEdge,
boolean fFlipDirection)
The list item
License requirements: nx_masterfem ("Finite Element Modeling") . |
DependentMeshListItemBuilder |
DependentMeshListItemBuilderList.findItem(int index)
Returns the object at the input index.
|
DependentMeshListItemBuilder[] |
DependentMeshListItemBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
DependentMeshListItemBuilderList.append(DependentMeshListItemBuilder object)
Appends an object to the list
License requirements: None. |
void |
DependentMeshListItemBuilderList.append(DependentMeshListItemBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
DependentMeshListItemBuilderList.erase(DependentMeshListItemBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
DependentMeshListItemBuilderList.erase(DependentMeshListItemBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
DependentMeshListItemBuilderList.findIndex(DependentMeshListItemBuilder obj)
Finds the index where the input object appears.
|
void |
DependentMeshListItemBuilderList.insert(int location,
DependentMeshListItemBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
DependentMeshListItemBuilderList.setContents(DependentMeshListItemBuilder[] objects)
Sets the contents of the entire list.
|
void |
DependentMeshListItemBuilderList.swap(DependentMeshListItemBuilder object1,
DependentMeshListItemBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.