Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static CorrelSolutionBuilder.EnumDampingFrftype |
CorrelSolutionBuilder.EnumDampingFrftype.FROM_WORK_MODEL
from work model
|
static CorrelSolutionBuilder.EnumDampingFrftype |
CorrelSolutionBuilder.EnumDampingFrftype.SPECIFY_DAMPING
from user input
|
Modifier and Type | Method and Description |
---|---|
CorrelSolutionBuilder.EnumDampingFrftype |
CorrelSolutionBuilder.frfDampingSource()
Returns the option controlling which damping to consider when synthesizing FRF data from analysis results
License requirements: None. |
static CorrelSolutionBuilder.EnumDampingFrftype |
CorrelSolutionBuilder.EnumDampingFrftype.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CorrelSolutionBuilder.EnumDampingFrftype |
CorrelSolutionBuilder.EnumDampingFrftype.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CorrelSolutionBuilder.EnumDampingFrftype[] |
CorrelSolutionBuilder.EnumDampingFrftype.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CorrelSolutionBuilder.setFrfDampingSource(CorrelSolutionBuilder.EnumDampingFrftype frfDampingSource)
License requirements: nx_correl_base ("FE Correlation") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.