Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static ConvertToConvergentBodyBuilder.Option |
ConvertToConvergentBodyBuilder.Option.COMPONENT_OF_CADBODY
The orginal component inside of assembly that polygon body is derived from in FEM Part
|
static ConvertToConvergentBodyBuilder.Option |
ConvertToConvergentBodyBuilder.Option.EXISTING_PART
The existing part where the convergent body in the FEM part will be exported to
|
static ConvertToConvergentBodyBuilder.Option |
ConvertToConvergentBodyBuilder.Option.NEW_PART
The new part where the convergent body in the FEM part will be exported to
|
static ConvertToConvergentBodyBuilder.Option |
ConvertToConvergentBodyBuilder.Option.PARENT_OF_FEM
The immediate parent of the current FEM Part
|
Modifier and Type | Method and Description |
---|---|
ConvertToConvergentBodyBuilder.Option |
ConvertToConvergentBodyBuilder.targetOption()
Returns the target option which indicates where the resulting convergent body will be created
License requirements: None. |
static ConvertToConvergentBodyBuilder.Option |
ConvertToConvergentBodyBuilder.Option.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ConvertToConvergentBodyBuilder.Option |
ConvertToConvergentBodyBuilder.Option.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ConvertToConvergentBodyBuilder.Option[] |
ConvertToConvergentBodyBuilder.Option.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ConvertToConvergentBodyBuilder.setTargetOption(ConvertToConvergentBodyBuilder.Option targetOptions)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.