Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static ConflictResolutionBuilder.Rule |
ConflictResolutionBuilder.Rule.ADD_DOF_VALUES
add dof values on the intersection
|
static ConflictResolutionBuilder.Rule |
ConflictResolutionBuilder.Rule.APPLY_FIRST_BC
apply first BC on the intersection
|
static ConflictResolutionBuilder.Rule |
ConflictResolutionBuilder.Rule.APPLY_SECOND_BC
apply second BC on the intersection
|
static ConflictResolutionBuilder.Rule |
ConflictResolutionBuilder.Rule.AVERAGE_DOF_VALUES
average dof values on the intersection
|
static ConflictResolutionBuilder.Rule |
ConflictResolutionBuilder.Rule.IGNORE_CONFLICT
specify dof values on the intersection
|
static ConflictResolutionBuilder.Rule |
ConflictResolutionBuilder.Rule.SPECIFY_DOF_VALUES
specify dof values on the intersection
|
Modifier and Type | Method and Description |
---|---|
ConflictResolutionBuilder.Rule |
ConflictResolutionBuilder.resolveRule()
Returns the resolution rule which will be used to resolve the conflict between the two input BCs
License requirements: None. |
static ConflictResolutionBuilder.Rule |
ConflictResolutionBuilder.Rule.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ConflictResolutionBuilder.Rule |
ConflictResolutionBuilder.Rule.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ConflictResolutionBuilder.Rule[] |
ConflictResolutionBuilder.Rule.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ConflictResolutionBuilder.setResolveRule(ConflictResolutionBuilder.Rule resolutionRule)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.