Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static CircularImprintBuilder.AroundEdgeDiaType |
CircularImprintBuilder.AroundEdgeDiaType.ABSOLUTE
Absolute Diameter Value
|
static CircularImprintBuilder.AroundEdgeDiaType |
CircularImprintBuilder.AroundEdgeDiaType.RELATIVE
Relative Value
|
Modifier and Type | Method and Description |
---|---|
CircularImprintBuilder.AroundEdgeDiaType |
CircularImprintBuilder.aroundEdgeDiaOption()
Returns an around edge dia option
License requirements: None. |
static CircularImprintBuilder.AroundEdgeDiaType |
CircularImprintBuilder.AroundEdgeDiaType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CircularImprintBuilder.AroundEdgeDiaType |
CircularImprintBuilder.AroundEdgeDiaType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CircularImprintBuilder.AroundEdgeDiaType[] |
CircularImprintBuilder.AroundEdgeDiaType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CircularImprintBuilder.setAroundEdgeDiaOption(CircularImprintBuilder.AroundEdgeDiaType methodOption)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.