Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static CfdLocalResolutionConstraintBuilder.ResolutionDensity |
CfdLocalResolutionConstraintBuilder.ResolutionDensity.SIZEIN_BOUNDING_BOX |
static CfdLocalResolutionConstraintBuilder.ResolutionDensity |
CfdLocalResolutionConstraintBuilder.ResolutionDensity.SIZEIN_BOUNDING_SPHERE |
static CfdLocalResolutionConstraintBuilder.ResolutionDensity |
CfdLocalResolutionConstraintBuilder.ResolutionDensity.SIZEON_ELEMENTS |
static CfdLocalResolutionConstraintBuilder.ResolutionDensity |
CfdLocalResolutionConstraintBuilder.ResolutionDensity.SIZEON_OBJECTS |
Modifier and Type | Method and Description |
---|---|
CfdLocalResolutionConstraintBuilder.ResolutionDensity |
CfdLocalResolutionConstraintBuilder.resolutionDensityType()
Returns the resolution density type
License requirements: None. |
static CfdLocalResolutionConstraintBuilder.ResolutionDensity |
CfdLocalResolutionConstraintBuilder.ResolutionDensity.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CfdLocalResolutionConstraintBuilder.ResolutionDensity |
CfdLocalResolutionConstraintBuilder.ResolutionDensity.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CfdLocalResolutionConstraintBuilder.ResolutionDensity[] |
CfdLocalResolutionConstraintBuilder.ResolutionDensity.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CfdLocalResolutionConstraintBuilder.setResolutionDensityType(CfdLocalResolutionConstraintBuilder.ResolutionDensity resolutionDensityType)
License requirements: nx_adv_fld_mod_solv ("NX Advanced Fluid Modeling - Full") OR sc_acou_meshing (" SC Acoustic Meshing") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.