Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static CfdContactPreventionConstraintBuilder.Contact |
CfdContactPreventionConstraintBuilder.Contact.CONTACTBETWEEN_ELEMENTS |
static CfdContactPreventionConstraintBuilder.Contact |
CfdContactPreventionConstraintBuilder.Contact.CONTACTBETWEEN_OBJECTS |
Modifier and Type | Method and Description |
---|---|
CfdContactPreventionConstraintBuilder.Contact |
CfdContactPreventionConstraintBuilder.contactType()
Returns the contact type
License requirements: None. |
static CfdContactPreventionConstraintBuilder.Contact |
CfdContactPreventionConstraintBuilder.Contact.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CfdContactPreventionConstraintBuilder.Contact |
CfdContactPreventionConstraintBuilder.Contact.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CfdContactPreventionConstraintBuilder.Contact[] |
CfdContactPreventionConstraintBuilder.Contact.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CfdContactPreventionConstraintBuilder.setContactType(CfdContactPreventionConstraintBuilder.Contact contactType)
License requirements: nx_adv_fld_mod_solv ("NX Advanced Fluid Modeling - Full") OR sc_acou_meshing (" SC Acoustic Meshing") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.