Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static CfdAutoRefinementConstraintBuilder.LocalSubdivisions |
CfdAutoRefinementConstraintBuilder.LocalSubdivisions.FIVE
Five levels of subdivision
|
static CfdAutoRefinementConstraintBuilder.LocalSubdivisions |
CfdAutoRefinementConstraintBuilder.LocalSubdivisions.FOUR
Four levels of subdivision
|
static CfdAutoRefinementConstraintBuilder.LocalSubdivisions |
CfdAutoRefinementConstraintBuilder.LocalSubdivisions.ONE
One level of subdivision
|
static CfdAutoRefinementConstraintBuilder.LocalSubdivisions |
CfdAutoRefinementConstraintBuilder.LocalSubdivisions.THREE
Three levels of subdivision
|
static CfdAutoRefinementConstraintBuilder.LocalSubdivisions |
CfdAutoRefinementConstraintBuilder.LocalSubdivisions.TWO
Two levels of subdivision
|
static CfdAutoRefinementConstraintBuilder.LocalSubdivisions |
CfdAutoRefinementConstraintBuilder.LocalSubdivisions.ZERO
No local subdivision
|
Modifier and Type | Method and Description |
---|---|
CfdAutoRefinementConstraintBuilder.LocalSubdivisions |
CfdAutoRefinementConstraintBuilder.localSubdivision()
Returns the maximum local subdivision
License requirements: None. |
static CfdAutoRefinementConstraintBuilder.LocalSubdivisions |
CfdAutoRefinementConstraintBuilder.LocalSubdivisions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CfdAutoRefinementConstraintBuilder.LocalSubdivisions |
CfdAutoRefinementConstraintBuilder.LocalSubdivisions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CfdAutoRefinementConstraintBuilder.LocalSubdivisions[] |
CfdAutoRefinementConstraintBuilder.LocalSubdivisions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CfdAutoRefinementConstraintBuilder.setLocalSubdivision(CfdAutoRefinementConstraintBuilder.LocalSubdivisions localSubdivision)
License requirements: nx_adv_fld_mod_solv ("NX Advanced Fluid Modeling - Full") OR sc_acou_meshing (" SC Acoustic Meshing") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.