Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
CAEVertex[] |
EdgePathMethod.PathEdgesData.pathstartvertices
resultant start vertices
|
CAEVertex[] |
EdgePathMethod.SeedEdgesData.seedstartvertices
seed start vertices
|
CAEVertex[] |
EdgePathMethod.SeedsData.seedstartvertices
seed start vertices
|
Modifier and Type | Method and Description |
---|---|
CAEVertex[] |
RelatedVertexMethod.getVertices()
Returns the resultant vertices
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
EdgePathMethod.addSeedEdge(CAEVertex seedStartVertex,
CAEEdge seedEdge)
Deprecated.
Deprecated in NX10.0.0. Use overloaded
EdgePathMethod.addSeedEdge(nxopen.cae.CAEVertex, nxopen.cae.CAEEdge) with additional arguments instead.
|
void |
EdgePathMethod.addSeedEdge(CAEVertex seedStartVertex,
CAEEdge seedEdge,
boolean preferFreeEdges,
boolean allowGapJumping,
double gapJumpingTolerance)
Add seed (start vertex and edge) to the end of the path.
|
EdgePathMethod |
SmartSelectionManager.createEdgePathMethod(CAEEdge seedEdgeTag,
CAEVertex seedStartVertexTag)
Deprecated.
Deprecated in NX10.0.0. Use overloaded
SmartSelectionManager.createEdgePathMethod(nxopen.cae.CAEEdge, nxopen.cae.CAEVertex) which takes as input an array of CAEEdge objects and the argument doEntityVisibilityCheck.
|
EdgePathMethod |
SmartSelectionManager.createEdgePathMethod(CAEEdge seedEdgeTag,
CAEVertex seedStartVertexTag,
boolean preferFreeEdges,
boolean allowGapJumping,
double gapJumpingTolerance)
Creates an edge path method
License requirements: nx_masterfem ("Finite Element Modeling") . |
RelatedEdgeMethod |
SmartSelectionManager.createRelatedEdgeMethod(CAEVertex[] seeds,
boolean doEntityVisibilityCheck)
Creates a related edge method
License requirements: nx_masterfem ("Finite Element Modeling") . |
void |
AbstractionManager.edgeMerge(CAEVertex[] ptVertex,
double vertexAngle,
boolean vertexAngleToggle)
Edge Merge
License requirements: nx_masterfem ("Finite Element Modeling") . |
void |
SetManager.setTargetSetEdgePath(int setIndex,
CAEEdge[] seedEdges,
CAEVertex[] seedVertices)
Deprecated.
Deprecated in NX10.0.0. Use overloaded
SetManager.setTargetSetEdgePath(int, nxopen.cae.CAEEdge[], nxopen.cae.CAEVertex[]) with additional arguments instead.
|
void |
SetManager.setTargetSetEdgePath(int setIndex,
CAEEdge[] seedEdges,
CAEVertex[] seedVertices,
boolean[] preferFreeEdges,
boolean[] allowGapJumping,
double[] gapJumpingTolerance)
Sets the CAE edge path in the specified set
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.