Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static CAEConnectionBuilder.ConnectionTypeEnum |
CAEConnectionBuilder.ConnectionTypeEnum.EDGE_TO_EDGE
between edges
|
static CAEConnectionBuilder.ConnectionTypeEnum |
CAEConnectionBuilder.ConnectionTypeEnum.EDGE_TO_FACE
between edges and faces
|
static CAEConnectionBuilder.ConnectionTypeEnum |
CAEConnectionBuilder.ConnectionTypeEnum.ELEMEDGE_TO_ELEMFACE
between element edges and faces
|
static CAEConnectionBuilder.ConnectionTypeEnum |
CAEConnectionBuilder.ConnectionTypeEnum.NODE_TO_NODE
between nodes
|
static CAEConnectionBuilder.ConnectionTypeEnum |
CAEConnectionBuilder.ConnectionTypeEnum.POINT_TO_EDGE
between points and edges
|
static CAEConnectionBuilder.ConnectionTypeEnum |
CAEConnectionBuilder.ConnectionTypeEnum.POINT_TO_FACE
between points and faces
|
static CAEConnectionBuilder.ConnectionTypeEnum |
CAEConnectionBuilder.ConnectionTypeEnum.POINT_TO_POINT
between points
|
Modifier and Type | Method and Description |
---|---|
CAEConnectionBuilder.ConnectionTypeEnum |
CAEConnectionBuilder.type()
Returns the connection type
License requirements: None. |
static CAEConnectionBuilder.ConnectionTypeEnum |
CAEConnectionBuilder.ConnectionTypeEnum.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CAEConnectionBuilder.ConnectionTypeEnum |
CAEConnectionBuilder.ConnectionTypeEnum.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CAEConnectionBuilder.ConnectionTypeEnum[] |
CAEConnectionBuilder.ConnectionTypeEnum.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CAEConnectionBuilder.setType(CAEConnectionBuilder.ConnectionTypeEnum connectionType)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.