Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static BoltBuilder.BoltOperation |
BoltBuilder.BoltOperation.BOLT_NUT
Creates a bolt connection with nut
|
static BoltBuilder.BoltOperation |
BoltBuilder.BoltOperation.BOLT_TAP
Creates a bolt connection in a tapped hole
|
static BoltBuilder.BoltOperation |
BoltBuilder.BoltOperation.SPIDER_JUNCTION
Creates a spider connection at junctions
|
Modifier and Type | Method and Description |
---|---|
BoltBuilder.BoltOperation |
BoltBuilder.operationType()
Returns the operation type
License requirements: None. |
static BoltBuilder.BoltOperation |
BoltBuilder.BoltOperation.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BoltBuilder.BoltOperation |
BoltBuilder.BoltOperation.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BoltBuilder.BoltOperation[] |
BoltBuilder.BoltOperation.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BoltBuilder.setOperationType(BoltBuilder.BoltOperation operationType)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.