Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static BeamSectionOffsetOptions.Method |
BeamSectionOffsetOptions.Method.LANGUAGE_SPECIFIC
The offset coordindate system is defined in language-specific way.
|
static BeamSectionOffsetOptions.Method |
BeamSectionOffsetOptions.Method.NEUTRAL
The offset coordindate system is defined in neutral way
|
Modifier and Type | Method and Description |
---|---|
BeamSectionOffsetOptions.Method |
BeamSectionOffsetOptions.offsetMethodType()
Returns the method to define beam end offsets
License requirements: None. |
static BeamSectionOffsetOptions.Method |
BeamSectionOffsetOptions.Method.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BeamSectionOffsetOptions.Method |
BeamSectionOffsetOptions.Method.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BeamSectionOffsetOptions.Method[] |
BeamSectionOffsetOptions.Method.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BeamSectionOffsetOptions.setOffsetMethodType(BeamSectionOffsetOptions.Method method)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.