Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static BaseFemPart.AxisymAbstractionType |
BaseFemPart.AxisymAbstractionType.NONE
No axisymmetric elements are allowed
|
static BaseFemPart.AxisymAbstractionType |
BaseFemPart.AxisymAbstractionType.XXY_PLANE
XY plane - X axis axisymmetric elements are allowed
|
static BaseFemPart.AxisymAbstractionType |
BaseFemPart.AxisymAbstractionType.XY_PLANE
XY plane - Y axis axisymmetric elements are allowed
|
static BaseFemPart.AxisymAbstractionType |
BaseFemPart.AxisymAbstractionType.ZX_PLANE
ZX plane - Z axis axisymmetric elements are allowed
|
Modifier and Type | Method and Description |
---|---|
BaseFemPart.AxisymAbstractionType |
BaseFemPart.getAbstractionType()
Gets axisymmetric abstraction type assoicated with the BaseFem part
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
static BaseFemPart.AxisymAbstractionType |
BaseFemPart.AxisymAbstractionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BaseFemPart.AxisymAbstractionType |
BaseFemPart.AxisymAbstractionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BaseFemPart.AxisymAbstractionType[] |
BaseFemPart.AxisymAbstractionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FemPart.finalizeCreation(Part cadPart,
String idealizedPartName,
FemPart.UseBodiesOption useBodiesOption,
Body[] bodies,
FemSynchronizeOptions geometrySyncOptions,
String solverTypeName,
String analysisTypeType,
BaseFemPart.AxisymAbstractionType abstractionType,
String[] description)
Deprecated.
Deprecated in NX10.0.0. Use
FemPart.finalizeCreation(nxopen.cae.FemCreationOptions) that takes FemCreationOptions as an input argument.
|
void |
FemPart.finalizeCreation(Part cadPart,
String idealizedPartName,
FemPart.UseBodiesOption useBodiesOption,
Body[] bodies,
FemSynchronizeOptions geometrySyncOptions,
String solverTypeName,
String analysisTypeType,
BaseFemPart.AxisymAbstractionType abstractionType,
String[] description,
boolean isMorphEnabled)
Deprecated.
Deprecated in NX11.0.0. Use
FemPart.finalizeCreation(nxopen.cae.FemCreationOptions) that takes FemCreationOptions as an input argument.
|
void |
AssyFemPart.finalizeCreation(Part cadPart,
String solverTypeName,
String analysisTypeType,
BaseFemPart.AxisymAbstractionType abstractionType,
String[] description)
Deprecated.
Deprecated in NX11.0.0. Use
AssyFemPart.finalizeCreation(nxopen.Part, java.lang.String, java.lang.String, nxopen.cae.BaseFemPart.AxisymAbstractionType, java.lang.String[], boolean, nxopen.CoordinateSystem) that includes CyclicSymmetryCSYS instead.
|
void |
AssyFemPart.finalizeCreation(Part cadPart,
String solverTypeName,
String analysisTypeType,
BaseFemPart.AxisymAbstractionType abstractionType,
String[] description,
boolean useCyclicSymmetryCSYS,
CoordinateSystem cyclicSymmetryCsys)
Finalizes the creation of the assembly fem part file.
|
void |
FemPart.finalizeCreationManaged(Part cadPart,
boolean createIdealPart,
FemPart.UseBodiesOption useBodiesOption,
Body[] bodies,
FemSynchronizeOptions geometrySyncOptions,
String solverTypeName,
String analysisTypeType,
BaseFemPart.AxisymAbstractionType abstractionType,
String[] description)
Deprecated.
Deprecated in NX11.0.0. Use
FemPart.finalizeCreation(nxopen.cae.FemCreationOptions) that takes FemCreationOptions as an input argument.
|
void |
BaseFemPart.setSolverAndAnalysisTypeAndAbstraction(String solverTypeName,
String analysisTypeName,
BaseFemPart.AxisymAbstractionType abstractionType)
Sets solver and analysis type and axisymmetric abstraction associated with the BaseFem part
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
FemCreationOptions.setSolverOptions(String solverName,
String analysisType,
BaseFemPart.AxisymAbstractionType abstractionType)
Set Solver, Analysis Type, and Axisymmetric Abstraction Type
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.