Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static AutomaticMorphBuilder.OrphanNodeMovementType |
AutomaticMorphBuilder.OrphanNodeMovementType.BASED_ON_NBR_MOVEMENT
Based on adjacent nodes movement.
|
static AutomaticMorphBuilder.OrphanNodeMovementType |
AutomaticMorphBuilder.OrphanNodeMovementType.STATIONARY
Stationary in topologically modified region.
|
Modifier and Type | Method and Description |
---|---|
static AutomaticMorphBuilder.OrphanNodeMovementType |
AutomaticMorphBuilder.OrphanNodeMovementType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AutomaticMorphBuilder.OrphanNodeMovementType |
AutomaticMorphBuilder.OrphanNodeMovementType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AutomaticMorphBuilder.OrphanNodeMovementType[] |
AutomaticMorphBuilder.OrphanNodeMovementType.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.