Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static AttachElementsBuilder.AttachOption |
AttachElementsBuilder.AttachOption.SPLIT_AND_ATTACH
split and attach
|
static AttachElementsBuilder.AttachOption |
AttachElementsBuilder.AttachOption.SPLIT_ONLY
split only
|
Modifier and Type | Method and Description |
---|---|
AttachElementsBuilder.AttachOption |
AttachElementsBuilder.attachType()
Returns an attach option
License requirements: None. |
static AttachElementsBuilder.AttachOption |
AttachElementsBuilder.AttachOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AttachElementsBuilder.AttachOption |
AttachElementsBuilder.AttachOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AttachElementsBuilder.AttachOption[] |
AttachElementsBuilder.AttachOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AttachElementsBuilder.setAttachType(AttachElementsBuilder.AttachOption attachmentType)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.