Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static AfuMathOperation.TimeToSrsResponseType |
AfuMathOperation.TimeToSrsResponseType.ABSOLUTE_MAX
Absolute Maximum
|
static AfuMathOperation.TimeToSrsResponseType |
AfuMathOperation.TimeToSrsResponseType.NEGATIVE_MAX
Negative Maximum
|
static AfuMathOperation.TimeToSrsResponseType |
AfuMathOperation.TimeToSrsResponseType.POSITIVE_MAX
Positive Maximum
|
Modifier and Type | Method and Description |
---|---|
static AfuMathOperation.TimeToSrsResponseType |
AfuMathOperation.TimeToSrsResponseType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AfuMathOperation.TimeToSrsResponseType |
AfuMathOperation.TimeToSrsResponseType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AfuMathOperation.TimeToSrsResponseType[] |
AfuMathOperation.TimeToSrsResponseType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AfuMathOperation.timeToSrs(String inputAfuFileName,
int inputRecordId,
double dampingRatio,
AfuMathOperation.TimeToSrsAxisType freqAxisType,
double frequencyMin,
double frequencyMax,
double frequenceIncrement,
int pointsPerDecades,
AfuMathOperation.TimeToSrsResponseType responseType,
String outputAfuFileName,
String outputRecordName)
Convert Time to SRS
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.