Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static AfuMathOperation.SrsToTimeOctave |
AfuMathOperation.SrsToTimeOctave.ONE_SIXTH
1/6 Octave
|
static AfuMathOperation.SrsToTimeOctave |
AfuMathOperation.SrsToTimeOctave.ONE_THIRD
1/3 Octave
|
static AfuMathOperation.SrsToTimeOctave |
AfuMathOperation.SrsToTimeOctave.ONE_TWELFTH
1/12 Octave
|
Modifier and Type | Method and Description |
---|---|
static AfuMathOperation.SrsToTimeOctave |
AfuMathOperation.SrsToTimeOctave.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AfuMathOperation.SrsToTimeOctave |
AfuMathOperation.SrsToTimeOctave.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AfuMathOperation.SrsToTimeOctave[] |
AfuMathOperation.SrsToTimeOctave.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AfuMathOperation.srsToTime(String inputAfuFileName,
int inputRecordId,
AfuMathOperation.SrsToTimeOption conversionOption,
double dampingRatio,
int numTimePoints,
int iterations,
AfuMathOperation.SrsToTimeOctave octave,
int numTrials,
AfuMathOperation.SrsToTimeStrategy strategy,
boolean saveSrsResults,
String outputAfuFileName,
String outputRecordName)
Convert SRS to Time
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.