Package | Description |
---|---|
nxopen.cae.aerostructures |
Provides classes and interfaces relating to Aero Structures.
|
Modifier and Type | Field and Description |
---|---|
static MarginCalculationBuilder.CalculationStatus |
MarginCalculationBuilder.CalculationStatus.ERROR
error
|
static MarginCalculationBuilder.CalculationStatus |
MarginCalculationBuilder.CalculationStatus.NOT_RUN
has not run
|
static MarginCalculationBuilder.CalculationStatus |
MarginCalculationBuilder.CalculationStatus.SUCCESS
success
|
Modifier and Type | Method and Description |
---|---|
MarginCalculationBuilder.CalculationStatus |
MarginCalculationBuilder.status()
Returns the execution status
License requirements: nx_masterfem ("Finite Element Modeling") . |
static MarginCalculationBuilder.CalculationStatus |
MarginCalculationBuilder.CalculationStatus.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MarginCalculationBuilder.CalculationStatus |
MarginCalculationBuilder.CalculationStatus.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MarginCalculationBuilder.CalculationStatus[] |
MarginCalculationBuilder.CalculationStatus.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MarginCalculationBuilder.setStatus(MarginCalculationBuilder.CalculationStatus cstatus)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.