Package | Description |
---|---|
nxopen.cae.aerostructures |
Provides classes and interfaces relating to Aero Structures.
|
Modifier and Type | Method and Description |
---|---|
MarginCalculation |
MarginCalculationCollection.cloneCalculation(String name,
MarginCalculation sourcemargincalculation)
Makes a copy the calculation and add it to the margin solution, replaces the given name if it is a duplicate
License requirements: nx_masterfem ("Finite Element Modeling") . |
MarginCalculation |
MarginCalculationCollection.findObject(String name)
Finds the
MarginCalculation object with the given name. |
Modifier and Type | Method and Description |
---|---|
MarginCalculation |
MarginCalculationCollection.cloneCalculation(String name,
MarginCalculation sourcemargincalculation)
Makes a copy the calculation and add it to the margin solution, replaces the given name if it is a duplicate
License requirements: nx_masterfem ("Finite Element Modeling") . |
MarginCalculationBuilder |
MarginCalculationCollection.createMarginCalculationBuilder(MarginCalculation margincalculation)
Creates a
MarginCalculationBuilder
License requirements: nx_masterfem ("Finite Element Modeling") Created in NX12.0.0 |
MarginResultTableDataProvider |
MarginSolution.createMarginResultTableDataProvider(MarginCalculation[] marginCalculations)
Creates a
MarginResultTableDataProvider
Only the subset of calculation given in argument are taken into account rather than all the calculation of the solution. |
void |
MarginCalculationCollection.deleteCalculation(MarginCalculation margincalculation)
Removes the calculation from the solution
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.