Package | Description |
---|---|
nxopen.cae.aerostructures.author |
Provides classes and interfaces relating to Aero Structures Author.
|
Modifier and Type | Method and Description |
---|---|
ABB.MsBoltCombinedShearTensionData |
ABB.msBoltCombinedShearTension(double iPTensileAllowable,
double[] iPTensileX,
double iPShearAllowable,
double factor,
double[] iPy,
double[] iPz)
MS bolt combined shear tension
Computes margin of safety of a bolt under shear load and tension load
The formula is 'MS = 1 / sqrt( Rt ^ 2 + Rs ^ 3 ) - 1'
where
Rt = PTensileX/PTensileAllowable
Rs = PShear/PShearAllowable
'PTensileAllowable' is the tensile load allowable of the bolt
'PTensileX' is the tensile load applied on the fastener
'PShearAllowable' is the single shear load allowable of the bolt
'Pshear' is the shearing load applied through the shear area.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.