Package | Description |
---|---|
nxopen.cae.aerostructures.author |
Provides classes and interfaces relating to Aero Structures Author.
|
Modifier and Type | Method and Description |
---|---|
ABB.MaterialFsyEstimationData |
ABB.materialFsyEstimation(double iFtyL,
double iFtyLT,
double iFcyL,
double iFcyLT,
double iFsu,
double iFtuL,
double iFtuLT)
Estimation of shear yield stress (Fsy)
Shear yield stress allowable ('Fsy') is estimated on the basis of the following formula:
'Fsy=( FtyL + FtyLT + FcyL + FcyLT ) / 4 * ( 2 * Fsu)/( FtuL + FtuLT )'
where:
'FtyL' is the tensile yield stress under longitudinal direction
'FtyLT' is the tensile yield stress under long transverse direction
'FcyL' is the compressive yield stress under longitudinal direction
'FcyLT' is the compressive yield stress under long transverse direction
'Fsu' is the shear ultimate stress
'FtuL' is the tensile ultimate stress under longitudinal direction
'FtuLT' is the tensile ultimate stress under long transverse direction
Input
FtyL Tensile yield stress, longitudinal direction
FtyLT Tensile yield stress, long transverse direction
FcyL Compressive yield stress, longitudinal direction
FcyLT Compressive yield stress, long transverse direction
Fsu Shear ultimate stress
FtuL Tensile ultimate stress, longitudinal direction
FtuLT Tensile ultimate stress, long transverse direction
Output
Fsy Shear yield stress
Return
Status of the calculation
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.