Package | Description |
---|---|
nxopen.cae.aerostructures.author |
Provides classes and interfaces relating to Aero Structures Author.
|
Modifier and Type | Method and Description |
---|---|
ABB.LoadDistributionBoltsConcentricLoadsData |
ABB.loadDistributionBoltsConcentricLoads(double[] p,
double[] iPsn,
int nblcXnbbolt)
Computes bolt loads for multiple bolt fitting - Concentric load
Formula
Pn = P * (Psn / SUM(Psn))
where:
'P' is the load acting on the fitting
'Psn' is the allowable strength of bolt n
'Pn' is the shear load on bolt n
Input
nblc Number of load cases
P Load acting on fitting (nblc)
nbbolt Number of bolts
Psn Allowable shear strength of bolt (nbbolt)
Output
Pn Shear load on bolt (nblc x nbbolt)
Return
Status of the calculation
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.