public static class ResultsEnvelopeBuilder.Operation extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_MAXIMUM |
static int |
_MINIMUM |
static ResultsEnvelopeBuilder.Operation |
MAXIMUM |
static ResultsEnvelopeBuilder.Operation |
MINIMUM |
Modifier and Type | Method and Description |
---|---|
static ResultsEnvelopeBuilder.Operation |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ResultsEnvelopeBuilder.Operation |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ResultsEnvelopeBuilder.Operation[] |
values()
Returns an array that contains the values for this enum.
|
public static final ResultsEnvelopeBuilder.Operation MINIMUM
public static final ResultsEnvelopeBuilder.Operation MAXIMUM
public static final int _MINIMUM
public static final int _MAXIMUM
public static ResultsEnvelopeBuilder.Operation valueOf(int value)
public static ResultsEnvelopeBuilder.Operation valueOf(String name)
public static ResultsEnvelopeBuilder.Operation[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.