public static class NodalForceReportBuilder.Force extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_APPLIED |
static int |
_CONTACT |
static int |
_GLUE |
static int |
_GRID_POINT |
static int |
_MPC |
static int |
_REACTION |
static NodalForceReportBuilder.Force |
APPLIED |
static NodalForceReportBuilder.Force |
CONTACT |
static NodalForceReportBuilder.Force |
GLUE |
static NodalForceReportBuilder.Force |
GRID_POINT |
static NodalForceReportBuilder.Force |
MPC |
static NodalForceReportBuilder.Force |
REACTION |
Modifier and Type | Method and Description |
---|---|
static NodalForceReportBuilder.Force |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NodalForceReportBuilder.Force |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NodalForceReportBuilder.Force[] |
values()
Returns an array that contains the values for this enum.
|
public static final NodalForceReportBuilder.Force GRID_POINT
public static final NodalForceReportBuilder.Force REACTION
public static final NodalForceReportBuilder.Force MPC
public static final NodalForceReportBuilder.Force APPLIED
public static final NodalForceReportBuilder.Force GLUE
public static final NodalForceReportBuilder.Force CONTACT
public static final int _GRID_POINT
public static final int _REACTION
public static final int _MPC
public static final int _APPLIED
public static final int _GLUE
public static final int _CONTACT
public static NodalForceReportBuilder.Force valueOf(int value)
public static NodalForceReportBuilder.Force valueOf(String name)
public static NodalForceReportBuilder.Force[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.