Package | Description |
---|---|
nxopen.bodydes |
Provides classes and interfaces for Body Design.
|
Modifier and Type | Field and Description |
---|---|
static OnestepUnformBuilder.Convergency |
OnestepUnformBuilder.Convergency.HIGH
Onestep solver convergency level is high
|
static OnestepUnformBuilder.Convergency |
OnestepUnformBuilder.Convergency.LOW
Onestep solver convergency level is low
|
static OnestepUnformBuilder.Convergency |
OnestepUnformBuilder.Convergency.MEDIUM
Onestep solver convergency level is medium
|
Modifier and Type | Method and Description |
---|---|
OnestepUnformBuilder.Convergency |
OnestepUnformBuilder.solverConvergencyLevel()
Returns the convergency level of onestep solver.
|
static OnestepUnformBuilder.Convergency |
OnestepUnformBuilder.Convergency.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OnestepUnformBuilder.Convergency |
OnestepUnformBuilder.Convergency.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OnestepUnformBuilder.Convergency[] |
OnestepUnformBuilder.Convergency.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OnestepUnformBuilder.setSolverConvergencyLevel(OnestepUnformBuilder.Convergency solverConvergencyLevel)
License requirements: nx_onestep_analysis ("NX Onestep Analysis") OR nx_general_packaging ("NX General Packaging") OR die_engineering ("DIE ENGINEERING") OR aero_sheet_metal ("Aerospace Sheet Metal") OR adv_sheet_metal_dsgn ("ADVANCED SHEET METAL DESIGN") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.