Package | Description |
---|---|
nxopen.blockstyler |
Provides classes and interfaces for Block Styler.
|
Modifier and Type | Field and Description |
---|---|
static Node.DropType |
Node.DropType.AFTER
Drop permitted after the target node
|
static Node.DropType |
Node.DropType.BEFORE
Drop permitted before the target node
|
static Node.DropType |
Node.DropType.BEFORE_AND_AFTER
Drop permitted before and after the target node
|
static Node.DropType |
Node.DropType.NONE
Drop not permitted
|
static Node.DropType |
Node.DropType.ON
Drop permitted on the target node
|
Modifier and Type | Method and Description |
---|---|
Node.DropType |
Tree.IsDropAllowedCallback.isDropAllowedCallback(Tree tree,
Node node,
int columnID,
Node targetNode,
int targetColumnID)
Represents the callback which gets called when an attempt is made to drop the node on any target node.
|
static Node.DropType |
Node.DropType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Node.DropType |
Node.DropType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Node.DropType[] |
Node.DropType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
boolean |
Tree.OnDropCallback.onDropCallback(Tree tree,
Node[] node,
int columnID,
Node targetNode,
int targetColumnID,
Node.DropType dropType,
int dropMenuItemId)
Represents the callback which gets called when nodes are dropped on any target node.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.