public static interface Tree.AskEditControlCallback
Tree.setEditOptions(java.lang.String[], int)
in this callback to show the options in the
edit-control. Further BlockStyler.Tree.OnEditOptionSelectedCallback is called when option is selected.Modifier and Type | Method and Description |
---|---|
Tree.ControlType |
askEditControlCallback(Tree tree,
Node node,
int columnID)
Represents the callback which gets called when edit is attempted on any cell.
|
Tree.ControlType askEditControlCallback(Tree tree, Node node, int columnID) throws NXException, RemoteException
Tree.setEditOptions(java.lang.String[], int)
in this callback to show the options in the
edit-control. Further BlockStyler.Tree.OnEditOptionSelectedCallback is called when option is selected.
tree
- Tree.node
- Node being edited.columnID
- Column Id of the column on which edit is performed.NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.