Package | Description |
---|---|
nxopen.assemblies.productinterface |
Provides classes and interfaces for Assembly Product Interfaces.
|
Modifier and Type | Field and Description |
---|---|
static ObjectBuilder.Mate |
ObjectBuilder.Mate.NO_CHECK
no checking for product interface objects
|
static ObjectBuilder.Mate |
ObjectBuilder.Mate.PREVENT
restrict user from using non product interface objects
|
static ObjectBuilder.Mate |
ObjectBuilder.Mate.WARN
warn user while using non product interface objects
|
Modifier and Type | Method and Description |
---|---|
ObjectBuilder.Mate |
ObjectBuilder.mateSetting()
Returns the current rule setting for use during creation of mating conditions
License requirements: None. |
static ObjectBuilder.Mate |
ObjectBuilder.Mate.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ObjectBuilder.Mate |
ObjectBuilder.Mate.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ObjectBuilder.Mate[] |
ObjectBuilder.Mate.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ObjectBuilder.setMateSetting(ObjectBuilder.Mate mateSetting)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.